1/31/2024 8:37 AM | |
Posts: 1 Rating:
|
Hello everyone, I'm currently facing an issue with communication between a K3 LINERFREE printer from Custom and a Unified panel. My goal is to establish a connection between these two devices via USB for printing purposes. I notice that on the panel, under the “Apps” and “Printer Configuration” tabs, the K3 LINERFREE printer is not listed. Only another Custom printer is present, but using it does not solve the problem. I'm reaching out to the community for assistance in finding a solution to this communication problem between the K3 LINERFREE printer and the Unified panel via USB. Is it possible to manually add a printer driver? Are there alternative connection methods besides USB that I could explore? Printer reference: 911HM011200733 - CUSTOM K3 HIGH SPEED LINERFREE Panel reference 1: 6AV2128-3GB06-0AX1 – MTP700 Unified Comfort Panel reference 2: 6AV2128-3UB06-0AX1 – MTP1900 Unified Comfort
Thank you in advance for your suggestions and expertise! Best regards, Attachmentimage.pdf (275 Downloads) |
Last edited by: Mehdi_Iteca at: 01/31/2024 08:38:07 |
|
Follow us on