3/13/2025 10:00 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! In the end, the main solution today is to use the siemens software with those operating systems that have been tested for compatibility, such as version 23H2. It is very likely that they are working on declaring compatibility with Windows in a future Update of V20, because if you check the excel of the compability tool there are many operating systems that are only compatible with certain versions of TIA Portal from a certain Update. If you are really interested in using the 24H2 version I suggest you to open a Support Request and probably they can give you more detailed information. |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on