11/20/2024 8:36 AM | |
Joined: 1/21/2013 Last visit: 9/17/2025 Posts: 4110 Rating:
|
Hi Jleon87, This is an international forum, so the forum language is English. Please keep this in mind when posting.
When you run the Doc Viewer (LibreOffice) application, you can see that the application is installed in a limited scope. It only comes with the Writer and Calc modules, others are missing. However, to execute your command, the Draw module is required, and since it is not available, your command will fail. However, you have not described the exact reason why you are attempting this file conversion. Have you tried using the lp command for direct printing?
Kind regards PS: WinCC Unified does not support the console object, so using it on the panel will not help you get additional information from your script, use the "Trace" method instead. |
Follow us on