11/11/2024 12:16 PM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! In principle, there shouldn't be any problem. Remember to set the Logo as LOGO! 8.FS4 in the configuration. I am attaching more information about it. Additionally, if you encounter any errors, please upload them as they will surely be helpful for people browsing the forum. - Why can you not download any programs into your new LOGO! 8?
|
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
11/11/2024 12:26 PM | |
Joined: 10/26/2013 Last visit: 5/17/2025 Posts: 63 Rating:
|
LOGO! 8.FS4 is not the same as LOGO 8.4. You neet to select the correct hardware in LogoSoft 8.4 |
11/11/2024 1:10 PM | |
Joined: 12/18/2014 Last visit: 9/7/2025 Posts: 35933 Rating:
|
If you want to communicate between LSC and a LOGO! 8.4 then need you the LSC version V8.4. You can update/upgrade any older version of LSC to the current version V8.4.1 for free. The update/upgrade can you download from here: Firmware update for LOGO! 8.4 basic devices and service pack 1 for LOGO! Soft Comfort V8.4If you have install the update/upgrade then load your program and select in the hardware selection the right LOGO! type LOGO! 8.4. |
11/28/2024 6:21 AM | |
Joined: 5/22/2024 Last visit: 12/21/2024 Posts: 2 Rating:
|
To resolve your issue, ensure your PLC firmware matches the Logo! Soft Comfort 8.4 software version. Update the PLC firmware to 8.4 if possible or open the 8.3 project in the 8.4 software, re-save it, and try downloading it again. On a lighter note, while troubleshooting, consider relaxing with the DixMax APK, an app for streaming movies and TV shows, which could be a nice break from technical tasks! |
Last edited by: barimitch at: 12/21/2024 05:40:02 |
|
Follow us on