11/7/2014 6:49 PM | |
Posts: 5 Rating:
|
HI to all, I am new in plc s7400. I have a question about the firmware for one CPU 414-15H PN/DP (6ES7 414-5HM06-A0B0), as following: Is possible to recovery the firmware ( in this case V6.0.0), from CPU of PLC?. It is because of in the "Module Information" asked me do one "Boot Loader" from V6.0.3 to V6.0.0. The same problem I have with CP 443-1 (6GK7 443-1EX30-0XE0) and CP 443-5. (6GK7 443-5DX05-0XE0) Attachment one picture. Thank you in advance and I hope your help Attachmenterror.zip (466 Downloads) |
Last edited by: Min_Moderator at: 11/10/2014 8:46 AMSplitted |
|
Follow us on