6/30/2010 8:18 AM | |
Posts: 621 Rating:
|
Hi all can any one know how to create an NCM file? with COM Profibus.(s7-200 plc) best regards algudkar |
11/1/2010 2:16 PM | |
Posts: 378 Rating:
|
I have the same question. Can any body can help? |
11/1/2010 4:14 PM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12407 Rating:
|
Hello desmul24; Could you please explain exactly you intend to do with this NCM file, in conjunction with a S7-200? I ask because to my knowledge the NCM database format file is used to download a Profibus configuration to a CP 5412 A2 processor for a PC,as a master for Profibus-DP and Profibus-FMS. Look at the following description from the Com Profibus manual: Export data to a NCM file You need binary databases in NCM format for SIMATIC NET PC modules (e.g. for the CP 5412 (A2)). The FILE> Export >NCM file function allows you to create databases in NCM format with COM PROFIBUS. You can then use the Service >Setting the PG/PC Interface function to load a database created in this way to a locally installed module. If you have installed a corresponding SIMATIC NET PC module, and one of the following products is also installed, COM PROFIBUS offers you the Export and Load NCM File functions in the pop-up menu for the module. This allows you to create a database and load it to the module immediately without having to use the Setting the PG/PC Interface function. PG-5412/Windows 98, NT 4.0 As of V 5.1 DP-5412/Windows 98, NT 4.0 As of V 5.1 FMS-5412/Windows 98, NT 4.0 As of V 5.1 SOFTNET-DP/ Windows 98,NT 4.0 As of V 5.1 http://support.automation.siemens.com/WW/view/en/1498610 Please forward more precise information on your application. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/1/2010 4:15 PM |
|
Follow us on