5/23/2019 10:20 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Hi Ipermix, very nice that you want to share your knowledge with the others, I appreciate it In addition to #dP's suggestion you can also create a thread in the Step7 TIA conference and mark them as a tip, too. You can forward this thread in the "feedback" box, which can be found under each manual/ documentation at the Product Support site. Best regards, Jen_Moderator |
5/23/2019 10:30 AM | |
Posts: 2826 Rating:
|
Dear Moderator, |
4/4/2024 6:34 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, "Function blocks" is the wrong directory (even if the block is an FB). The important thing in your case: You have to use the folder "Library Types". This is also the case if the type is used in the project and the help is called from the type from project. SIMATIC STEP 7 Basic/Professional V18 and SIMATIC WinCC V18regards sancruz |
Last edited by: sancruz at: 04/04/2024 06:36:04Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
Follow us on