6/16/2017 4:12 AM | |
Joined: 7/13/2011 Last visit: 9/4/2025 Posts: 37 Rating:
|
Dear Experts, i need some clarification about CU250S_2DP controller(Sinamics G120) with 1FT6 motor. 1. Configuration is Speed control Application = CU250S-2DP(V4.7) + PM240-2 + SMC20 + 1FT6 Motor with Absolute Encoder. 2. First time i am doing configuration with factory reset, Encoder is configured with drivecliq communication with SMC20 automatically. 3. Then I try to configure motor data i select in Wizard--> select motor from list--> Synchronous motor--> then i will select motor with code number(P301) 4. After this configuration all my motor data including encoder data is automatically set OK. 5. My problem is after changing my motor details from induction motor to Synchronous motor with motor code number, control modeautomatically changed from P1300=21(SVC) to P1300= 20(SLVC). Then i can not able to change with Speed control with encoder(P1300=21), it's always showing error while i try to change P1300 from 20(SLVC) to 21(SVC). 6. My question is Cu250S can possible synchronous servo motor with encoder option. I am confused what will be the problem. 7. I tried many ways to change the control mode in,, BOP and Via Scout software and offline configuration & download... etc. But not possible to change my control mode Give me solution for my problem ASAP. For refference i attached project backup. Thanks in advance Regards Gopinath AttachmentFeeding_Roll_CU250S.zip (124 Downloads) |
Follow us on