11/21/2018 2:02 PM | |
Posts: 69 Rating:
|
In manual on library i read that i can create xml file APLCustomerUnits.xml i create that file and put to OS project in GraCS folder. https://support.industry.siemens.com/cs/ww/en/view/109482346/0 After that i modify Unit number in block And after that he in APL write that undefined units Anyone know this is bug or need somewere inicialize APLCustomerUnits.xml file. |
Last edited by: Tmsoft at: 11/21/2018 2:03:04 PMLast edited by: Tmsoft at: 11/21/2018 2:06:04 PMLast edited by: Jen_Moderator at: 11/22/2018 12:48:44 PMOptimized link. |
|
11/21/2018 3:55 PM | |
Posts: 69 Rating:
|
I also trying Mvar Units and nothing I attach my example xml file Yes before the starting Wincc i put in GraCS folder that xml and after that i start, wincc starting wihout any errors, but XML dosent work, i know also that if you change in xml file units you must restart Wincc, but it feels like he doesn't even see this configuration. I think this is a Wincc bug AttachmentAPLCustomerUnits.zip (245 Downloads) |
Last edited by: Tmsoft at: 11/21/2018 3:56:23 PMLast edited by: Tmsoft at: 11/21/2018 3:57:50 PMLast edited by: Tmsoft at: 11/21/2018 4:01:27 PMLast edited by: Tmsoft at: 11/21/2018 4:01:57 PMLast edited by: Tmsoft at: 11/21/2018 4:02:59 PM |
|
11/22/2018 10:34 AM | |
Posts: 69 Rating:
|
Thank you but i also testing on English language too and nothing, anyway you can test by your way and you will see. |
11/22/2018 1:05 PM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hi Tmsoft, why you want to change the unit with a xml-scpirt? An easy why to change an unit of an APL-block is with the input "XX_Unit" of the block . Usually you can write an Integer number for the units. The number of the most commonly units you can find in the Manual Advanced Process Library. Is the unit not in the list of commonly units you can write "0" at the input and open the properties of the input "XX_Unit". In Properties of the input you find the dropdownlist "Unit" there you can write your own Unit. After an compile and download of the AS and OS the change are visible at the OS. with regards |
Last edited by: Heisenberg2 at: 11/22/2018 1:23:29 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on