10/3/2024 8:16 AM | |
Joined: 5/27/2024 Last visit: 8/26/2025 Posts: 54 Rating:
|
Hi, I need to retrieve alarm bits from the slave PLC S7-300 for the master device. In which data block should I add the alarm data? Can I use the instance data block of MODB_341 for this, or do I need to create a separate data block (source DB)? I'm using TIA Portal. Note: Communication - Modbus RTU Slave, RS 485 Interface Hardware - In slave side ( S7-300 + CP-341 + Slave Dongle ) Software - TIA portal V13. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/04/2024 07:34:40New subject after splitting |
|
Follow us on