7/12/2017 4:50 PM | |
Posts: 1 Rating:
|
Hello Mr Pegagia, I'm using Optimised DB with a S7-1500 CPU and I need programing Bit Alarms in the HMI, but I can't do it. I don't know what is the "Trigger variable" . Can you help me? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/13/2017 11:02:07 AMNew subject after splitting |
|
7/20/2017 4:47 PM | |
Posts: 648 Rating:
|
Dear chidt, if the "Trigger variable" ist true the alarm will be triggert. With best regards rh1990 |
7/20/2017 11:05 PM | |
Joined: 11/16/2012 Last visit: 8/21/2025 Posts: 307 Rating:
|
The trigger variabel is a word variable. You can either set it Bit wise if you are using slice access. See: How in STEP 7 (TIA Portal) do you access the unstructured data types bit-by-bit, byte-by-byte or word-by-word and symbolically? Or you can use overlaying with the AT keyword. See: How do you program the overlaying of tags with the keyword "AT" in the STEP 7 (TIA Portal)?
|
Follow us on