10/30/2024 2:55 PM | |
Joined: 5/22/2017 Last visit: 6/8/2025 Posts: 7 Rating:
|
Hi I was able to download the program but the error still appears. is that normal? |
10/30/2024 3:46 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, You can use TIA Portal v18 or higher, then it is part of TIA Portal Or you can use GSDML file: PROFINET GSD files: I/O – ET 200SP Best regards, Wizard |
10/31/2024 6:19 AM | ||||||||||||
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, at first the diagnostics window shows 2 different things, unfortunately it can be confusing how its done. 1. Additional information: Anything stated below the additional information note, is just a information, not an error. Yes, you have to check if the modules are compatible. In this case, they are. Means you can configure the predecessor "old module" and use the successor "new module" in the real hardware. The new module is spare part compatible, means this does not cause the error above. 2. The error message: This can be connected, to the additional information. For example if in hw config the new module would be configured, but in the real hardware the old one was used. This way around, it would not be compatible. So if for an DI a newer firmware was configured as the module itself has, this also will lead into an error with online/offline difference shown in the interface module. Alternative approach: Delivery release for the innovated ET 200SP interface module IM 155-6 PN ST
-> yes, this will lead to the note in diagnostics page "online/offline" difference. But does not cause an error. 6ES7155-6AU02-0BN0
-> means only available in (up from) internal catalog of V18 -> but as an alternative, GSD can be used (install the GSD -> device can be found in "other field devices" folder). PROFINET GSD files: I/O – ET 200SPregards sancruz |
|||||||||||
Feedback appreciated, please rate |
||||||||||||
This contribution was helpful to
1 thankful Users |
Follow us on