6/12/2009 5:16 AM | |
Joined: 10/7/2005 Last visit: 8/28/2025 Posts: 3049 Rating:
|
Hello hefeng you need COM Profibus to configurean IM308Cor to read out the configuration of an IM308C (V5.1 is the latest, the configuration is not all that different from the HWconfig in Step7). You'll also either need a Profibus card in your laptop (e.g. CP5512) to be able to downloador upload to/from an IM308C or alternatively a Siemens PG or external USB prommer whichallows you read/writethe Flash Eprom of the IM308C. Which I/O addresses are used for what card in your ET200U stations is all contained (configured) in COM Profibus. The IM316 that you mention is however NOT a Profibus interface module but merely there to extend the local "rack" of a 90U or 95U or 100U (an IM318 is the Profibus interfacefor ET200U). Anyway, I hope this helps Cheers Fritz |
Cheers |
|
Follow us on