7/13/2017 11:02 PM | |
Joined: 9/2/2014 Last visit: 5/10/2025 Posts: 10 Rating:
|
Hi, Where can I find an example project with S7-400FH. ?I have S7-412-5H station running with a ET200 with redundancy bundle. I want to add a second ET200M station with Failsafe IO modules . I have the F- RT License and F-Library, CFC and Step 5.5 SP4 . But before I begin with, if I have an example project s7-400FH , that would help me to minimize errors and pitfalls. Thanks . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/14/2017 12:43:06 PMNew subject after splitting |
|
7/13/2017 11:28 PM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12407 Rating:
|
Hello Kamath; I think this Apllication Example should help you develop your configuration: Realization of a Fault-Tolerant Tunnel Lighting System With S7-400H The solution realized in this application example offers the following advantages:
Hope this helps, Daniel Chartier |
7/14/2017 8:41 AM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Dear User, There is an example for FH systems, but you need to install the components first to be able to view the safety-related program.The projects are available after installation of software package.You need to check this Manual and the following for passwords to handle it. opening ZEn32_02_FSystem_FHProj exampleI hope it helps, hdhosseini |
This contribution was helpful to
1 thankful Users |
Follow us on