12/13/2011 9:30 PM | |
Joined: 12/22/2010 Last visit: 10/21/2022 Posts: 10 Rating:
|
Dear All, Need your kind support and urgent help to solve the subject fault in Masterdrive VC(CUVC). There are two pumps drives (PM 3568B & A) in which one of the pump drive is in standby and one is running depending on the process requirement. For pump drive B- Fault F021 is appearing immediate on OP1S when the motor is running on full rpm (3600 rpm) but it is running smoothly when motor is running with 50% of rpm. For pump drive A- It is running smoothly with full rpm now it is running continously but now we fear that if any problem occur than we will face a big problem and we cannot run pump drive B in full speed. Please find attached complete parameter for your kind reference. Regards, fasi457 AttachmentPM3568B-131211@14.30.pdf (443 Downloads) |
Follow us on