12/1/2024 3:36 PM | |
Joined: 7/29/2019 Last visit: 8/25/2025 Posts: 10 Rating:
|
Hello everyone, I hope you're all having a good day. Request you to Pls download attachment for better understanding of concern. I have a question regarding the "Value field-Drawing field" signals in CAEX Logic Chart. Specifically, I want to know if there's a way to select multiple signals within a specific POU and use a "Find and Replace" method to quickly update the text inside the selected Value field for the selected POUs only. Here’s the situation: I'm required to make around 1000 logics with each logic having multiple inputs and outputs connected to a single block. I’ve standardized the names of different signals, with each signal being differentiated by a unique number (since multiple signals and logics are used) Now, I have a few logic, and now I copy and pasted it for all 1000 logic. However, the inputs and outputs for each logic need to be updated based on the unique numbers for each signal. The text of the Value fields are standardized and only the numerical number needs to be updated. Instead of manually renaming each signal one by one, I’m looking for a more efficient way to automate this process, like using a "Find and Replace" technique, if possible. In my first attachment, you can see that all the signals are the same across each of the 1000 logics, except for the numerical part. I’ve already imported all the signals into the Variable Declaration Editor, so now I just need a way to quickly update the signal names across all the logics. AttachmentAttachment for clarity on concern.docx (202 Downloads) |
Follow us on