5/19/2020 4:59 PM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
https://support.industry.siemens.com/cs/pd/113014?pdti=td&dl=es&lc=es-WW Yes it should work. You can you configure the x4 S7-200 in the software -- right? Regards. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
5/19/2020 5:17 PM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12407 Rating:
|
Translation from the Spanish message:
Hola Petruler; Este foro de Siemens atrae a participantes de muchos paises, y no todos entienden el español. Para facilitar nuestros encuentros, hemo escogido el inglés como idioma común. Hazos el favor de escribirnos en inglés a tu próxima visita. Gracias. Hello Petruler; The siemens forum attracts members from many countries, and not all of them understands Spanish. To make our exchanges easier, we have selected English as our common language. Please write to us in English on your next visit. This link gives a possible solution, and it is in Spanish (bonus!). When ypu have done the TIA Portal configuration, start by attributing (in Microwin) a different address for each S7-200 CPU): http://www.tecnoplc.com/comunicacion-mpi-hmi-s7-200-tia-portal/ Notice: Establecida la comunicación entre un HMI y un PLC para una red MPI, siempre teniendo en cuenta de no solapar ninguna dirección dentro la red, es decir, que siempre, cada estación (PLC, HMI, esclavo 1, esclavo 2…) debe tener un número diferente. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
5/19/2020 5:29 PM | |
Joined: 11/27/2019 Last visit: 10/9/2024 Posts: 5 Rating:
|
|
5/19/2020 5:32 PM | |
Joined: 11/27/2019 Last visit: 10/9/2024 Posts: 5 Rating:
|
thanks for the reply Hi. Yes I can configure the s7 200 with the Microwin. But what I want to do is communicate the 4 S7 200s with a single KTP400 HMI. From what I have seen I can configure different communication drivers and assign them an address. Then I could assign these addresses to the s7 200. My question is if this works or am I wrong
|
Follow us on