4/20/2016 8:20 AM | |
Joined: 12/16/2012 Last visit: 9/8/2025 Posts: 655 Rating:
|
Hi! "When multiple registers (words) are to be transferred, with the "MB_HOLD_REG" parameter the symbolic name of an array, struct or PLC data type that covers the specified data volume of the master (DATA_ADDR and DATA_PTR) must be transferred. The first word of this array, struct or PLC data type corresponds to the MODBUS holding register start address 40001." how-do-you-establish-a-modbus-rtu-communication-with-step-7-(tia-portal)-for-the-simatic-s7-1200 |
This contribution was helpful to
1 thankful Users |
4/24/2016 12:09 PM | |
Joined: 8/8/2014 Last visit: 9/12/2022 Posts: 34 Rating:
|
Thank Kahl. I got it |
This contribution was helpful to
2 thankful Users |
Follow us on