4/21/2017 3:16 PM | |
Posts: 648 Rating:
|
Dear Nattana, https://support.industry.siemens.com/cs/ww/en/view/109742302/86055241099 and https://support.industry.siemens.com/cs/ww/en/view/68014632 could be helpful. With best regards rh1990 |
5/16/2017 2:46 PM | |
Joined: 1/30/2006 Last visit: 5/15/2025 Posts: 310 Rating:
|
What do your Faceplate do. You have the Faceplate Scripts |
BR. Sven |
|
5/18/2017 1:01 PM | |
Posts: 2 Rating:
|
First off thanks for your swift reply and suggestions. I guess I did not elaborate my problem well. I know that global VBs cannot be used inside faceplates and I am also using UDT that contains all my motor info and am using them in my motor global DB. My problem is that I have excess of over 250 motors and each motor will have a faceplate that contains 3 buttons and each button will have 2 events each that will set/reset tags (start,stop...) in my UDT. If I could connect events to my buttons that will set/reset tags in UDT inside faceplate my work would be greatly reduced as I will just interface the faceplate with my motor number when I bring it to the screen but alas it seems impossible. So I have to connect tags to buttons of each motor individually in the event tab when I call my faceplate to the screen. That is really time consuming. As I had said I found out that it is possible to set/reset UDT tags in the events tab inside faceplate editor in Wincc Advanced (see in attachment). If only there was a way to do the same in Wincc Pro... Best Regards Salman
AttachmentFaceplate et UDT HMI_EN.pdf (328 Downloads) |
Follow us on