11/21/2012 2:49 PM | |
Joined: 10/14/2009 Last visit: 10/15/2024 Posts: 33 Rating:
|
When I copy the ET200L from the project that has a properly configured ET200L rack in it, I can edit it and save it and it retains the lines in the configuration enabling configuration of the individual SC modules in the SC rack. That looks like a nice workaround for the 6ES7-131-1BL11-0XB0, assuming that the SC terminal block used in that configuration is the same or compatible with the terminal block used in the system I am trying to fully convert to S7. Unfortunately, the project with properly configured ET200L SC IO does not have a rack with a 6ES7-131-1BH11-0XB0 module in it. Does anyone have a project with a properly configured 6ES7-131-1BH11-0XB0 module in it? Alternately, I am figuring that if I had a proper GSD file, a rack inserted from my catalog would come in with these lines to configure the SC IO. Unfortunately, all the GSD files I have found only have configuration information for about four lines. Does anyone know how to get a copy of a GSD file that would allow the IO to be configured, and then put it into my project, so I could pick it from the list? I tried to install all the ET200L racks available in Step7 5.5, and none of them conatined lines to configure the SC IO modules. For example, the GSD file here Order no.: 6ES7 131-1EH00-0XB0 http://support.automation.siemens.com/WW/view/en/113440 does not appear to have information for any more than four slots. I am not sure if those slots at the end of the configuration file correspond to the lines I need to configure the SC modules. So far that is just a hunch. Best Regards, Doug |
Last edited by: O_Moderator at: 11/22/2012 9:52 AMlink edited Last edited by: dougt at: 11/21/2012 2:56 PM |
|
Follow us on