6/29/2017 8:26 AM | |
Posts: 1 Rating:
|
Hi all, It someboday found way how to get UDT to Faceplate which is on Popup window? I have arround 20 artickel on faceplate so make multiplex tag for every artickel sounds for me like nightmare and I realy don't want to put valves or all analogs to array becouse than i can't give them name and code is with 100 valves not easy readable. Im working with Wincc Advanced V13 sp2 or V14 sp1. thanks Lenka ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/29/2017 3:49:17 PMNew subject after splitting |
|
6/29/2017 8:30 PM | |
Posts: 20 Rating:
|
Hi Lenka, You can copy your udt to the project library. After that use the udt from the library as properties tag of the faceplate. Then in the interface tab of the faceplates you connect which DB data it should show data from. This is only one way to do it. /David R |
6/29/2017 9:42 PM | |
Posts: 20 Rating:
|
here is a siemens quick tutorial on how it worksAttachment68014632_Faceplates_GettingStarted_en.pdf (844 Downloads) |
Follow us on