7/19/2019 4:54 PM | |
Posts: 1 Rating:
|
Hi, I just bought a Siemens S7-1500 PLC and am attempting to interface read/write variables from a Forte OPC-UA with the PLC. The problem is that the PLC has its own OPC-UA server. I am including pictures from my attempt. It seems as though the Forte server’s nodes have numeric ID , whereas Siemens’ are a string. Image 1 How do I declare the endpoint URL on the Client's FB ID to connect this variable on the Siemens PLC? Endpoint Used:
Image 2 Attachmentimages.zip (369 Downloads) |
Last edited by: Jen_Moderator at: 07/22/2019 08:03:54Removed links and added files as an attachment. |
|
7/20/2019 8:10 PM | |
Joined: 5/6/2010 Last visit: 9/12/2025 Posts: 2031 Rating:
|
Hello, maybe is this link with a lot of application examples helpful OPC UA application examples S7-1500 regards |
This contribution was helpful to
1 thankful Users |
Follow us on