5/19/2023 3:53 PM | |
Joined: 1/31/2019 Last visit: 6/26/2025 Posts: 2 Rating:
|
Hey guys, since I´m running into kind of the same issue, I´ll just try to ask you wether can point me in the right direction. I already created a batch file which is doing its work, if i start it via doubleclick. Here`s my script::)
Unfortunately it does not work as expected. I´m trying to run this script tied to a button click event in my HMI.That may be the issue? Should i create a separate script that i have to call in a certain way? Since this is the last thing, I do not have that much expertise I assume, that somewhere around here my issue is located. Any suggestions why it won´t work? I´d really appreciate your responses :-) ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_7929563 at: 05/19/2023 15:54:47Last edited by: Jen_Moderator at: 05/22/2023 11:26:29New subject after splitting |
|
7/18/2024 12:13 PM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16349 Rating:
|
Hello Do you use a PC RT or a Unifeid Panel? Do you have an application with Graphic frontend or without? If your program has a GUI then use this FAQ: https://support.industry.siemens.com/cs/de/en/view/109798677 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on