1/22/2009 9:42 AM | |
Posts: 122 Rating:
|
dear experts: when i executed the "block consistency check" and then compiled there are error generated which is showed in the drawing attached.the error is that"S7-PDIAG:Too many active error definitions". i want to ask what is the possible reason to this error and how can i solve this problem?thanks! AttachmentS7-PDIAG compiling error.zip (557 Downloads) |
1/23/2009 11:51 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, regarding to your inquiry we would like to inform you. We recommend to compile the program in S7-PDIAG. Open S7-PDIAG in the SIMATIC Manager with "Option > Configure Process Diagnostics". After use the function "Process Diagnostics > Compile Completely" in S7-PDIAG. The compilation in S7-PDIAG should be finished without errors. In this case repeat the "Check Block Consistency" again. Consider:
Further informations you will see in the FAQ: With best regards |
1/29/2009 3:55 AM | |
Posts: 122 Rating:
|
dear expert: when i compiled completely inside the S7-PDIAG according to your suggestion the same error came out.please see the picture attached. Attachmentcompiling error1.zip (509 Downloads) |
Follow us on