10/21/2013 8:02 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hi LOGO! Soft comfort v8.0??? or you have LOGO! Soft Comfort v7 and windows 8? |
10/21/2013 10:17 AM | |
Joined: 11/23/2011 Last visit: 9/9/2025 Posts: 202 Rating:
|
Hello GeBairakt, please scroll in the menu to "Tools>Options>Interface" and proof if "LOGO! Cable is selected". There is also a button "Automatic detection" for the Interface. In addition have a look on the following FAQ How can you connect LOGO! with a PC?. When you scroll down in the FAQ there are some error messages than can occur when trying to get a connection and what you have to do. Please also navigate in your LOGO!Soft Comfort to the menu "Help>About". What version is displayed there, because I think you meant LOGO!Soft Comfort V7with Windows8 as Ste39 also mentioned. I hope this information helps you. Please inform us if your problem gets solved. Greetings, KM_AS |
This contribution was helpful to
1 thankful Users |
10/22/2013 3:16 PM | |
Posts: 7 Rating:
|
I have Logo!Soft Comfort version8.0, or at least that's what my computer says. |
10/22/2013 3:42 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, o.k. that's cleared, now the second problem, the interfaces look verry strange, did you install the cable drivers during instalation of Logosoft? If you have USB cable you can download the drivers here Regards, Marcjan |
Problem solved? |
|
10/22/2013 3:51 PM | |
Posts: 7 Rating:
|
I don't remember when I installed the drives. May I install them again ? |
Follow us on