2/28/2023 5:04 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
which tp700 exactly, can you post the order Number? |
This contribution was helpful to
1 thankful Users |
3/6/2023 11:08 AM | |
Joined: 8/3/2009 Last visit: 9/9/2025 Posts: 16368 Rating:
|
Hello Awint If you have a normal Comfort Panel then you can do the Reset to factory settings with a normal Ethernet Cable (It is made with MAC address): https://support.industry.siemens.com/cs/ww/en/view/19701610 You do not need another special cable! there are only a few situations in which a reset to factory settings does not work. What shows your panel display? does it run to Runtime or WinCE completly (then you should be able to do a Reset ) Or do you have a KTP700?? then It is a Basic Panel 2nd en and you have to use another way (USB Recovery) A few more information would help us to find the best solution Good Luck bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on