7/13/2023 8:02 AM | |
Joined: 3/25/2011 Last visit: 6/25/2025 Posts: 56 Rating:
|
Hi all! TIA V16 Upd5, CPU 1215C DC/DC/DC V4.4. When I set the DB block option to "Data block write-protected in the device", an error occurs. Why? The block is used in the function as an Input parameter. Data from the block is only read. --- [snip]
AttachmentFiles.zip (316 Downloads) |
Last edited by: ProgIga at: 07/13/2023 08:04:14Last edited by: Jen_Moderator at: 07/13/2023 11:41:50Links removed and files attached as .zip file. |
|
7/14/2023 6:49 AM | |
Joined: 3/25/2011 Last visit: 6/25/2025 Posts: 56 Rating:
|
I removed the "Writable from HMI/OPC UA/Web API" option for the UD_1 type. It did not help. Also, I removed this option from the tag with type UDT_1 in DB (I made a second DB, "Global DB"). It did not help. In the third DB "Global DB" the tag with type (standard array) has this option, but there is no error!
AttachmentProject2_20230714_0946.zip (337 Downloads) |
Last edited by: ProgIga at: 07/14/2023 08:06:53 |
|
Follow us on