9/15/2023 9:09 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello shehin I´m not sure about this combination. In the Compatibility tool you can see that only Con.Sation V7.5SP2 is released with WinCC V7.5SP2 and V7.5 SP1 with WinCC V7.5 SP1: https://support.industry.siemens.com/cs/ww/en/view/64847781 Bye Murof |
If this Information really helps, you could use the Rate function |
|
9/20/2023 12:10 PM | |
Joined: 1/20/2022 Last visit: 8/21/2025 Posts: 9 Rating:
|
Hi Mr.murof, Thanks for your kind information, If I configured SPOSA Application and download to connec station client will it work or i have to configure OPC server. And also can I download 2 different project to one connectivity station. |
Follow us on