8/31/2024 8:19 AM | |
Posts: 2 Rating:
|
Hello. I am using a new Logo 6ED1052-1MD08-0BA1 base module and I also have a 6ED1055-1NB10-0BA2 expansion module. The inputs and outputs are working on the base module and the inputs are working on the expansion, but the outputs are not working. I have search through the display and I can see the outputs Q5 to Q8 is on, and in the code it is also on but I'm not getting anything from the physical terminal output. Have you any advice on this please. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/02/2024 08:22:01New subject after splitting |
|
8/31/2024 11:04 AM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
Please don't post twice for the same problem. You also make a own topic: Logo Expansion outputs not working |
9/2/2024 8:23 AM | |
Joined: 7/30/2024 Last visit: 9/8/2025 Posts: 942 Rating:
|
Closed because posted twice. The active topic can be found here: Logo Expansion outputs not working Kind regards, Moderator_Lan |
Follow us on