7/10/2015 11:31 PM | |
Posts: 10 Rating:
|
is possible example I1 button on/off Q1,I2 button on/off Q2 en I3 button general on/ off Q1,Q2. Tanks but i can not
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/13/2015 9:09:57 AMNew subject after splitting Last edited by: Min_Moderator at: 7/13/2015 9:10:24 AM |
|
7/11/2015 3:58 PM | |
Posts: 10 Rating:
|
tank, but i can this table logic for 3 push ed 2 outpout whit logosoft V8?I can not do it.... |
7/11/2015 4:11 PM | |
Posts: 10 Rating:
|
this solution, for me, is not easy to use for a home automation solution without a signaling lamp on the button and also with the signal lamp is difficult
|
7/11/2015 4:48 PM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35925 Rating:
|
Try this. |
7/11/2015 6:05 PM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35925 Rating:
|
And for the logic table is the second example the correct one. |
This contribution was helpful to
1 thankful Users |
7/11/2015 9:08 PM | |
Posts: 10 Rating:
|
I1 start light Q1 I1 stop light Q1 I2 start light Q2 I2 stop light Q2 I3 as logic table |
7/12/2015 12:02 AM | |
Posts: 5225 Rating:
|
Hi. Aiuterà molto se si mostra un'immagine del sistema. ..regardless of an image to show us the design intent Please note that the system requires the release of a button before executing the requested task. It becomes difficult because the PLC do not know the intention of the human before he releases a button. Feel welcome to test the program and come back with commentary on where it does not work for you. My apologies for not taking too much time with documentation and making the circuit neat and human readable. Greetings. AttachmentDesign idea_Local and remote multi purpose buttons.zip (475 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on