4/5/2023 2:54 PM | |
Joined: 5/10/2022 Last visit: 4/6/2023 Posts: 3 Rating:
|
Hi, Experts: I got same another issue but cause the same result. Our power supply: 600VAC/400VAC Transformer, Filter, Inductance, then to SIMODRIVE 611 36kW.6SN1145-1BA02-0CA1 To 2U1,2V1,2W1, power supply 400VAC To 1U1, 1V1,1W1, power supply 420VAC we had another 5 machine like this. but this machine run with 28 axes. and right now machine only could run 40% rate. when over 40% we will get I/R module OverVoltage Faults. but all other machine it works fine, the power supply to 1U1,1V1,1W1 are 600VAC. Please help to check how it cause this. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/06/2023 09:30:50New subject after splitting |
|
4/6/2023 9:32 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject 840Di system Only work under 40% is published within the conference SINUMERIK CNC automation systems. Jen_Moderator |
Follow us on