8/26/2015 3:04 PM | |
Posts: 2 Rating:
|
Hi, I hope someone can help me here. I am making a simple machine to combine two liquids, a solvent and a type of adhesive, and want to use a logo8 + TDE to calculate and display the mix ratio. There are flow meters on each liquid which provide a pulse, corresponding to a certain amount of liquid. I need to determine the frequency of the pulses and calculate the flow rate, in mililitres/minute, for both liquids. Then perform another calculation to determine the ratio.
I will then manually adjust the pumps to achieve the correct proportions. However the mathematics instruction won't accept the pulse frequency in the calculation, so I can't get beyond this point. My program is attached. I must be doing something wrong but I'm totally stuck! How should I be doing this? Thanks! Tom. AttachmentMixer Display.zip (239 Downloads) |
8/26/2015 3:11 PM | |
Joined: 12/18/2014 Last visit: 9/9/2025 Posts: 35940 Rating:
|
Look here: |
This contribution was helpful to
1 thankful Users |
8/26/2015 3:42 PM | |
Posts: 2 Rating:
|
Great! Thanks a lot. I couldn't find this info anywhere. |
This contribution was helpful to
1 thankful Users |
Follow us on