6/30/2018 1:28 PM | |
Joined: 3/14/2008 Last visit: 9/1/2025 Posts: 2215 Rating:
|
Hi, The signal status 16#FF is default signal (not connected signal status). Please try one of the following byte values: 1 16#00 Bad, device related Normally,the generate module drivers function will connect the Mode. The mode is set according the connected hardware. If you remove the Mode connection and compile+download AS without Generating Module Drivers, you can simulate error by setting a wrong mode. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
7/1/2018 8:02 AM | |
Joined: 2/9/2012 Last visit: 8/15/2022 Posts: 32 Rating:
|
Here is what is displayed in the InstanceDB |
Follow us on