2/14/2017 3:54 PM | |
Joined: 3/1/2016 Last visit: 4/14/2025 Posts: 6 Rating:
|
Hi there, According to this topic it is possible to copy log files from the panel to a PC by just taking the SD-card and reading it on a PC. I would like to empty the file after the copy. Is there any procedure? Must the csv files have the first line (header line)? Can I just delete the files (move to the PC)? Have I to restart the panel? Have I to stop the logging, extract the SD-card and start the logging after having pluged the SD-card back in? I am working on a TP1200 with TIA Portal V13 SP1 Upd4. Regards, |
Last edited by: M_Franke at: 2/14/2017 3:55:31 PMLast edited by: M_Franke at: 2/21/2017 4:23:43 PM |
|
2/21/2017 4:23 PM | |
Joined: 3/1/2016 Last visit: 4/14/2025 Posts: 6 Rating:
|
Has anyone any idea? |
3/7/2017 11:53 AM | |
Joined: 3/1/2016 Last visit: 4/14/2025 Posts: 6 Rating:
|
Please? |
3/7/2017 3:27 PM | |
Joined: 8/3/2009 Last visit: 9/1/2025 Posts: 16284 Rating:
|
Hello M_Franke The workflow that you describe is not a clean one. I would connect the Panel with ethernet to a PC which has a shared folder: https://support.industry.siemens.com/cs/ww/en/view/92346478 then stop the loggin and close all logs and create a copy of the Logging to the Shared Folder like this: https://support.industry.siemens.com/cs/ww/en/view/63042926 Then Open logs and start logging and everything works fine without a huge interuption. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on