1/18/2019 3:12 PM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello you should do a Backup of the only Panel and do a restore in the new panel. This is the most simple way. If you do not have a Backup but only the Project then do the configuration of the new Panel to the same settings as the old was and then transfer the project again. https://support.industry.siemens.com/cs/ww/en/view/28928853 Bye Murof |
If this Information really helps, you could use the Rate function |
|
1/30/2019 11:33 AM | |
Posts: 14 Rating:
|
Connected via ethernet ip address |
Follow us on