6/29/2013 4:33 PM | |
Posts: 9 Rating:
|
Hello I`m a beginnerin this world of automation so my knowledge is very limited, but increasing....... I purchased a S7 1200 for testing my programs,soI have been programming for several weeks, and now, I would like to try with WinCC RT. I want to learn programming and SCADA simultaneously. I`m using Tia Portal V12 and WinCC Advanced.
I attached a pdf file that contains all the screens in the programming process from the beginning. I do not know what is happenning. I do not have any complete similarexample for comparing. AttachmentRuntime Example.zip (577 Downloads) |
6/29/2013 7:39 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, Have you gone through this important Tip published by Ganesh.
Also, you can refer entire Link Here Getting Started WinCC V12 |
VANDE MATARAM..... |
|
6/30/2013 10:23 AM | |
Posts: 9 Rating:
|
Thank you very much. I knew those documents. I actually checked them before posting, but I did not find any tips for fixing my problem. Note that the task I`m trying to do is much simpler than the one shown there. Thanks again. EER |
6/30/2013 12:31 PM | |
Joined: 4/17/2012 Last visit: 6/17/2025 Posts: 474 Rating:
|
Hi pls check here you will get the tag columns... if u click there you will get a list box there you have to select PLC connection or internal connection. external connection means from where you going to connect i.e PLC tag address that is called external connection
|
6/30/2013 7:12 PM | |
Posts: 9 Rating:
|
Maybe It was product of my ignorance. I thought I could do that way. I want the runtime to read the status of the bits I0.0 and Q0.5, in the program block Main OB1 that are bool tags. For that task I added two rectangles and set the Appearance like shown in the last pages of the attached document. I`m not using IO Fields anymore but It does not work anyway. What am I doing bad? Thank you AttachmentSample 20130630.zip (569 Downloads) |
Follow us on