1/13/2023 3:23 AM | |
Joined: 10/13/2021 Last visit: 8/21/2025 Posts: 8 Rating:
|
Stefan. Look please the attachment. BR, ilya. AttachmentInnovanc.zip (730 Downloads) |
1/13/2023 6:09 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4108 Rating:
|
Hi ilya, this forum is mainly used by volunteers. We can provide tips on how to solve problems, but you should not expect your work to be done by volunteers. Your project may be relevant at a later date, but it does not contain any of the items I last recommended for your review. Also, I can't open the project because it wasn't created to be language neutral, so it doesn't fit my system. To verify your project, you can create a new support request. But be aware that the support engineers also need relevant information like the diagnostic buffer. Kind regards |
1/18/2023 6:40 AM | |
Joined: 10/13/2021 Last visit: 8/21/2025 Posts: 8 Rating:
|
Hi Stefan. Thanks for you report. I changed code via you advice but it's not working. Thank you for your assistance. You can see the attached file AttachmentInnovanc.zip (799 Downloads) |
1/20/2023 3:34 AM | |
Joined: 10/13/2021 Last visit: 8/21/2025 Posts: 8 Rating:
|
Hello Stefan. it FC i tested with plc sim and physical cpu. And it request error (SF and CPUI going in stop mode). You can delete frequency converter in hardware, it's profibus device and does not affect on project. If you are interested, .gsd file in attachment AttachmentMD38DP2.zip (765 Downloads) |
1/20/2023 4:45 AM | |
Joined: 3/30/2020 Last visit: 9/15/2025 Posts: 5448 Rating:
|
@Dunaev-ik: Consider the offer that Mr. Stefan has put to you and follow the provided link to apply for a free support session. (See the quoted text below.)
Good luck. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
Follow us on