4/21/2009 4:41 PM | |
Joined: 9/27/2006 Last visit: 9/5/2025 Posts: 12398 Rating:
|
Hello Cranky; When you say "transfer your program from the WinCC to the PLC", do you plan on setting up communications between the 2 , or do you have something else in mind? If you want to communicate between the WinCC PC and the PLC, you can choose Ethernet or Profibus. Since you have a CPU 315-2DP, I would think you would want to use the integrated DP port on the PLC to achieve the link. You would then need a communication card on the PC (CP 5611 for example, or CP 5613) with the adequate driver. Profibus cable and connectors between the PC and the PLC, of course. Information on WinCC communications (Profibus amongst others)can be found in great detail in the following manual: http://support.automation.siemens.com/WW/view/en/21320307 Also check the WinCC online help, it is quite a good source opf information. A detailed description of the configuration of Profibus links is available in the WinCC Information System under "Communication > SIMATIC S7 Protocol Suite > Configuring the channel > Channel units > "PROFIBUS (I+II)" channel units"". Hope this helps, Daniel Chartier |
4/21/2009 5:14 PM | |
Posts: 8 Rating:
|
Thanks a lot for the link Chartier. I would like to ask if there is any link like this one when using the MPI connection?????????? Many Thanks |
4/21/2009 6:13 PM | |
Posts: 8 Rating:
|
Thanks again. How fustrating that can be. I have done almost everything said in the help menu as well as the link but still it doesn't work |
Follow us on