3/13/2019 6:49 PM | |||||
Joined: 3/28/2015 Last visit: 9/12/2025 Posts: 725 Rating:
|
Hello, Perhaps the following topics might help: 3-SIMATIC TD17, OP3, OP7 and OP17, Discontinuation effective 10/01/2007 Product (Discontinuation on 10/01/2007):
Recommended Replacement Model:
Backup/Restore with ProSave It is not possible to load and edit a backup file in ProTool or WinCC flexible.The file can only be reloaded to the original or another panel via a restore with ProSave. You need the Configuration program of the panel then you can change the panel type. Uploading the Configuration program only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable back transfer". |
||||
Eng.Mohamed Ibrahim |
|||||
Follow us on