2/22/2016 2:39 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Well, I made about 30 copies of the block... All in OB35 and everything OK (8.1 SP1) Do you have a screenshot of the block showing the runtime group in CFC? |
If I could help you, you can use the RATE button. Thank you. |
|
2/23/2016 7:29 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hello Skata, How are you? Do you have a screenshot of the CFC block? I think it's unlikely to have a block not inserted in OB3x in CFC. It should be indicated in the right upper part of the block. See the enclosed file. I'm very curious what it says on your "Trigger" block. Thanks! |
If I could help you, you can use the RATE button. Thank you. |
|
2/24/2016 12:48 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi PSW, Good that you recreated the initial problem. I was hoping for a screenshot to see what runtime group the block was set to. And indeed: Setting predecessor position to OB35 will have the following blocks inserted in runtime group OB35. Still hoping for an answer from Skata. |
If I could help you, you can use the RATE button. Thank you. |
|
3/8/2016 12:40 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
When you select: "Predesessor for insert position", did you select the first option: "OB33\<CFC chartname>?? When you select the other one-> OB100\<CFC chartname>, then the next block will install in OB100. So make sure you select "OB33" I cannot see perfectly in your attached picture, but the first block is inserted in OB33? Or OB32? If OB32, replace OB33 in the above text. |
If I could help you, you can use the RATE button. Thank you. |
|
5/27/2016 12:22 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hello! Well, this option is new since PCS7 v8.1. Default the setting is active (checked), but when you upgraded an older version to v8.1, the option can be checked manually. What it does is that an runtime group is created automatically for OB100. This will support the "Selective download" function, so that you are able to download only the changed charts. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on