12/16/2024 7:00 PM | |
Joined: 6/10/2024 Last visit: 12/20/2024 Posts: 3 Rating:
|
Hi, i am trying to install PLCsim advanced V5.0 but i always end up with an error in the last two minutes of installation I have checked the Log and all i can find is: 17:15:44 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 17:15:44 | FAIL!RebootAfterAll SetupUnit (PLCSIMADV_Driver64) Failed ClassicComponentAddLocal Is there anyone that has had the same problem and know how to fix this? Best regards, AttachmentSIA_S7-PLCSIM_Advanced_V5.0@24-12-16_17-12-58_AFTERREBOOT_summary.txt (487 Downloads) |
12/17/2024 9:06 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi AutoGen_1427825, In this case, the first thing I would check would be the operating system compatibility and the PLCSim V5.0 you are trying to install. What version of operating system are you using exactly? On the other hand: - Are you installing on some domain? - Do you have full administrator rights? Are you running the installation as administrator to have access to all folders on the PC? - From where are you installing PLCSim from a DVD or have you downloaded it from SIOS? We are waiting for this information! Recommendation -> Re-download the installation file to the C: drive and try again, making sure to install to the suggested default location. Best regards! |
If this Information really helps, you could use the Rate function |
|
12/18/2024 8:15 AM | |
Joined: 6/10/2024 Last visit: 12/20/2024 Posts: 3 Rating:
|
I have tried to restart the computer several times, i have also tried the update version of PLCSIM advanced v5_Update2, i have also tried to install V6 and V6Upd1 none have worked, getting the same error every time. I have also tried shutting down windows firewall during installation, still same error I am using the ISO file downloaded from siemens website I have attached the log files if you wish to see them to help me Best regards, AttachmentSIA_Starter.zip (338 Downloads) |
Last edited by: AutoGen_1427825 at: 12/18/2024 08:22:50Last edited by: AutoGen_1427825 at: 12/18/2024 09:16:59 |
|
This contribution was helpful to
1 thankful Users |
Follow us on