12/12/2012 4:01 AM | |
Posts: 15 Rating:
|
Hello everyone, Could somebodypleasehelp me with the following problem: I tried to connect to an existing project in MP-277 8" Touch and uploading the program in my PC using directEthernet connection (crossover cable)and WINCC flexible 2008. I set network IP in both equipment and I could ping to MP277, but when I tried to upload the project (back-transferring) an error message"could not find the plz file" shown and transfer failed. I tried it several time and checked every thing but that message apeared again, finally the transferring stopped in "establishing connection to device" and noyhing happend for while!! The attached file include the mentioned messages. Help please! Regards, ABSL Attachmentsiemens amcor.pdf (261 Downloads) |
12/12/2012 6:27 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Could be that the option With Backtransfer was not selected when project was downloaded. How do you back transfer the projects of an operator panel and what should you watch out for? If it fails again you can try to make a backup, only problem then is you cannot edit the project, just transfer it to same type of panel. How do you backup/restore with a Windows-based panel? Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to
1 thankful Users |
12/14/2012 4:06 PM | |
Posts: 3037 Rating:
|
Hello, There are no possibilities except backtransfer. Tweety |
2/27/2019 7:16 PM | |
Joined: 4/21/2015 Last visit: 5/4/2024 Posts: 8 Rating:
|
Hi, hope someones still in this room.? Can't we just use ProSave? |
Follow us on