7/8/2011 3:20 PM | |
Posts: 241 Rating:
|
Dear Maraitorzz......... Can you tell me which Interface module you are using , IM153-2 or IM157 , what is the type number of Y-coupler and Bus modules? I am also facing similar problem when I switch over Redundanct CPU, in my case after switchover communication becomes OK, All the inverters in the Y link tripped when I switchover. We are using IM153-2BA02-0XB0 with bus module:195-7HD80-0xa0 and 654-7HY00-0XA0 We have selected IM from DP/PA-link from Profibus-DP in the HW COnfig. splitted from Y-link redundancy fault. |
Last edited by: O_Moderator at: 7/11/2011 8:07 AMnew subject after splitting |
|
7/8/2011 5:49 PM | |
Posts: 241 Rating:
|
In my case I have IM153-2 but I am surprize when I see online Diagnostic: Why it is like this? |
Last edited by: PowerTags at: 7/8/2011 5:51 PMattch |
|
7/3/2014 3:05 PM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 24 Rating:
|
For me this is OK, once an Y-Linkwith DP/PA Link has 2 times IM53-2 and 1 DP/PA Coupler IM 157 in the rack. |
Follow us on