5/19/2009 2:01 PM | |
Posts: 38 Rating:
|
I have a weird problem. I'm trying to convert Protool project to WinCC flexible project but it is not working. I will get only an error notification when wincc is checking the consistency of the Protool project. I attached the output of the error notification. Hopefully someone knows what the problem is. I have tried the migration with other computers and they are working very well, so the problem is not in the protool-project. I also reinstalled all SIMATIC products but this didn't help either (I used this guide when I uninstalled all products http://support.automation.siemens.com/WW/view/en/189025). |
5/19/2009 3:05 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, Did you have also deinstalled WinCC flexible and use this cleanup tool? -> http://support.automation.siemens.com/WW/view/en/28465762 It is possible, that the version from the flexible did not supported the panel from ProTool --> Maybe it is a PC project and you did not have install flexible advanced. regards, |
Follow us on