6/28/2017 3:09 PM | |
Joined: 9/19/2016 Last visit: 6/7/2024 Posts: 30 Rating:
|
Dear all, We updated the simotion scout at the last version (simotion scout V4.5 SP1) the fist step of the updating was to update the step 7 at the V5.5 SP4 HF11 version and the second step was to update the simotion scout at the V4.5 SP1 version. After the installation we converted the project from V4.4 to V4.5 version and it is gone in the right mode. When we press the button 'save and build' the building stops at the 25 %, as in the picture. The compilation stops at the step: Generate symbolic assignment (25%) and the message inside the set output addresses is: drive Telegram uniformity with Config HW... To complete the information, inside of the CX172A1 there is a TM31 (as in the picture 2) with a imposed telegram from user, so we imposed a length of input and output data. The only way to unlock the situation is to kill the scout process. We noticed that when we the building stops at 25% a siemens process automatically dies, the name of this process is u7bt04ax.exe (I hope that this information is useful for you to understand the problem).
I hope that my description is clear. thanks a lot,
AttachmentErrors.zip (549 Downloads) |
6/28/2017 4:10 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, can you attach the project , or a sample project with this error? Christoph |
Follow us on