1/1/2014 10:05 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, When only a digit chnages, like here for 6ES7 307-1BA00-0AA0 and 6ES7 307-1BA01-0AA0, the second is mostly a successor/substitution type of the first one. Have a look to the "update" entries for SITOP on the support pages,. where they explain the order number changes, like this one: http://support.automation.siemens.com/WW/view/en/48986511 New versions are also announced via "delivery release" entries like this one: http://support.automation.siemens.com/WW/view/en/38626434 The 6ES7 307-1EA80-0AA0 is an outdoor version. http://support.automation.siemens.com/WW/view/en/4067761 On the support pages you can have a look to the tab "technical data", to see if the power supply matches your needs, like this one: http://support.automation.siemens.com/WW/view/en/37051064/td |
Best regards |
|
This contribution was helpful to
3 thankful Users |
1/16/2014 8:35 AM | |
Posts: 340 Rating:
|
new question is splittet to anybody having quick reference table for IO card ? |
Follow us on