11/18/2024 5:38 PM | |
Joined: 5/3/2021 Last visit: 12/2/2024 Posts: 1 Rating:
|
Hey, i am looking for help on implementing a Rice Lake SCT-2200 fieldbus module into one of my programs on TIA Portal. I have located the GSDML file and installed. I am just down to the programming at this point. I have the setup manual from rice like that lists the registers and the descriptions of the values. I am having trouble understanding how i should bring my weights into the program, they are made of three bytes with the first byte being MSB and the third byte being LSB. Also if there is any other info on implementing this scale in my program that would be much appreciated. I attached the fieldbus setup guide from rice lake.
AttachmentRice Lake Field Bus setup.pdf (226 Downloads) |
Follow us on