12/12/2013 12:37 PM | |
Posts: 81 Rating:
|
Hi everyone! I am using the S7-1200 1212DC/DC/DC cpu to count pulses on two inputs. The code involves counting of pulses on I0.0 in such a way that the pulse is counted for a second, once a second is completed the counter is reset to 0, the counted value is moved to another MW from where it is converted into a string, and then appended to another long string so that it contains 60 values, for 60 seconds. The issue is, the count is being missed. I have even tried simulating the count with using 2.5Hz internal clock but the values get Missed out. AttachmentKiwiPow_60sString1inputs.zip (454 Downloads) |
12/12/2013 2:25 PM | |
Joined: 7/27/2012 Last visit: 3/27/2025 Posts: 24 Rating:
|
Dont reset the counter just move the value, and divide the values, better to leave the counter running. |
Follow us on