9/11/2020 8:06 AM | |
Posts: 26 Rating:
|
Hello, Can someone explain, if possible, which is the cheapest way to connect S7-300 PLC with io-link IFM rotary encoder RV3500? Encoder's specification: https://www.ifm.com/gb/en/product/RV3500 Best regards, toby |
9/11/2020 2:04 PM | |
Joined: 9/9/2014 Last visit: 2/12/2025 Posts: 246 Rating:
|
Hello, look at the guides below Acyclic Read and Write with the IO-Link Library How do you determine the Vendor ID and the Device ID of an IO-Link device? If I were you, I would look towards the distributed periphery... Use ET200SP interface module and module CM 4xIO-Link (6ES7137-6BD00-0BA0 FW >= V2.2) The cost will be one of the cheapest solutions (for 300 series you can't imagine another) |
Best Regards |
|
This contribution was helpful to
1 thankful Users |
9/11/2020 3:11 PM | |
Joined: 9/21/2012 Last visit: 9/4/2025 Posts: 4703 Rating:
|
It depends, do you already have something else, than the CPU? Like a fieldbus for sensors? |
Follow us on