11/10/2011 5:44 AM | |
Joined: 3/24/2010 Last visit: 5/19/2025 Posts: 123 Rating:
|
Good day, I just want to seek an expert advise on this. I got an error which says "DP slave not accessible by means of the bus." I want to link my S5 ET200U (6es5-318-8mb12) to my S7 network but i keep on getting this error. I am using 313C-2 DP cpu. Please help me with this problem. I checked the dip switch for node address, ET200u is set to "3" and on my config the PLC is "2" the baud rate is 9.6kbps, but i started from 1.5mbps and it did not work. I know someone here can help me with this. thank you in advance. Daniel Attachmentpics.zip (361 Downloads) |
11/10/2011 12:19 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread S7-313C-2 DP to S5-ET200U remote I/O connection Best regards O_Moderator |
Follow us on